============================================================
                            InstaCal
                 Measurement Computing Corporation
     ============================================================


1. Introduction
2. Requirements
3. Known issue
4. Support policy and how to contact us


==========================================
1. Introduction
==========================================
Installation:
InstaCal is an easy to use installation, calibration and test utility 
for your data acquisition hardware. When you plug in your Measurement
Computing Hardware, InstaCal detects the hardware and assigns resources 
automatically. You may set special features of the hardware so your software 
programs will run as you wish. All the settings are stored in the 
Measurement Computing configuration file.

Calibration:
Once your board is installed, you may want to check calibration. 
InstaCal walks you through a professional calibration procedure tailored 
to the board you own.

Test:
InstaCal will test the board both internally and externally, giving you 
complete confidence in the board operation. If a problem is found, 
it is clearly identified which will speed a complete repair.


==========================================
2. Requirements
==========================================
  Microsoft Windows 10/8/7/Vista/XP operating system (32-bit/64-bit versions)*
   (Windows 7 requires SP1 and the latest Windows updates; XP requires SP3)
  Microsoft .NET Framework 1.1 or later (required for User's Guide installation)
  Intel Pentium III class processor, 500 MHz or higher 
  Video display800 x 600, 256 colors or greater
  Minimum of 256 MB of RAM (512 MB or higher recommended) 
  Minimum of 125 MB of free hard disk space 
  Microsoft-compatible mouse 
  Windows Installer version 1.1 or later 
   

* For 64-bit Vista operating systems, see the known issue below. ISA, PC104, PPIO, 
PC-CARD (and PCMCIA) and E-PDISO16 devices are not supported on Windows 10/8/7 and 
Windows Vista.
PCI-DAS1000/1200/1600 Series devices are not supported for 64-bit operating systems.


==========================================
3. Known issue
==========================================
Due to a driver compatibility issue, using InstaCal on Windows Vista 64-bit operating
system requires one of the following:

1. InstaCal version 6.55 or earlier, or 
2. Disable driver signing verification in Windows Vista 64 (using F8 at boot or bcdedit)


==========================================
4. Support policy and how to contact us 
==========================================
Please contact Measurement Computing for information 
on technical support.

Measurement Computing
10 Commerce Way
Norton, MA 02766
Phone: (508) 946-5100
Fax: (508) 946-9500
www.mccdaq.com

You may check for the latest version of InstaCal from our download site at 
http://www.mccdaq.com/software.aspx. 

InstaCal is a trademark of Measurement Computing Corporation.
Windows is a registered trademark of Microsoft Corporation.